5/29/2018 12:41 AM | |
Posts: 3 Rating:
|
Hello I want to communicate a vilter compressor panel with S7-1500 CPU by modbus TCP, but I have two errors 80C4 and 80C5, I used mbclient module, and I tested the communication with a modbus software on the PC, and PLC reads fine, but with panel cannot established comm. I tested with another client modbus software and I can read the panel's holding register, but between S7-1500 CPU and panel doesn´t work for now If someone could me help, I'll be grateful CPU serial: S7-1515-2PN Firmware version 2.1 Cordially Oscar Muñoz ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 5/29/2018 1:58:33 PMNew subject after splitting |
|
5/29/2018 5:30 PM | |
Posts: 3 Rating:
|
thanks for your answer, I have ID 1 in the TCON_IP_v4 parameters that configures the connect of MB_Client But not works for now |
10/3/2022 11:22 AM | |
Joined: 12/9/2020 Last visit: 12/8/2024 Posts: 17 Rating:
|
Thanks, Great people |
Follow us on