10/29/2020 11:53 AM | |
Posts: 12 Rating: (0) |
Every time I connect mysiwarexthe red led(DIAG) is on and gives me some errors which is shown in the attached image. 1- low limit violated when i connect sense + and - with exc + and - . 2- ( CPU error: New I/O access error during process image update output 104 (16 Bytes) will temporarily not be updated as part of process image PIP 0 PLC_1 / SIWAREX WP231.). pls i need help in connecting, configuration and programming iam usingcpu 12001214 dc/dc/dc andSIWAREX WP231. and TIA Portal 15.1. ty all^_^
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/29/2020 14:10:59New subject after splitting |
|
10/29/2020 2:11 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (173) |
Closed cause question posted twice. The second thread with the subject Siwarex Errors is published within the conference Process Instrumentation / Analytics / Weighing Systems SIWAREX. Best regards,Jen_Moderator |
Follow us on