8/22/2023 6:14 PM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928)
|
Hi, The master OS should have inserted: WinCC Application in the NetPro configuration. The Standby OS should have inserted: WinCC Application Standby inserted. There is only one project which will be downloaded to both servers. To do this, you select the OS station in component view->right click->PLC->Download. Do this for the master and Standby one after another.. after the first download you can also download changes which is executed by selecting the master OS and again right click on PLC->Download. The option changes is now possible (only when you compile OS changes and not a full compile which result that only a full download is possible) |
If I could help you, you can use the RATE button. Thank you. |
|