4/18/2012 8:28 AM | |
Joined: 7/3/2011 Last visit: 3/17/2025 Posts: 81 Rating:
|
Dear All, In my new project having the following configuration. 1. CPU 412- 2PN 2. ET 200 M Remote Station-A (9 DI modules and 3 DO Modules connected with PN (wired)) 3.ET 200 M Remote Station-B (10 AI Modules Connected with PN (Wired)) 4. ET200 M Remote Station-C (8DI Modules and 4 DO Modules connected with PN (Wireless)) 5.ET 200 M remote Station-D (3 DO modules and 6 AI Modules connected with PN (Wireless)) I am using the wireless communication for WLAN 786-1 Pro. There is no problem in to establish the wireless communication. My problem I cant able to access the Station-c and station-d digital output modules in cpu. There is no SF and BF in station C and D. But the SF in CPU also module not available (I/O Access error) in diagnosis message. If i will remove the all digital output modules in both station c and d there is no fault in CPU and its in run mode. If i will connect only one output modle in each station c and d there is no fault in ET 200 m and SF in CPU and its Stop mode. please give the suggestion for me to solve the issue. I am also changed my profinet I/O system updation times from upto 512 there is no changes. I have attached my configuration screen shots and online messages. please help me Regards AttachmentLMS CONFIGURATION.zip (144 Downloads) |
Follow us on