2/9/2017 7:34 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hi shoaib, S7-1200: Onboard 14 DI Extensions: Signalmodules: 8 signalmodules can have up to 8 AI or 16 DI But I would rather take a ET200SP. You have almost the same possibilities but it has a better performance. ET200SP: Maximum 12/32/64 I/O modules (depending on the CPU/interface module used, see CPU More infos about ET200SP: SIMATIC ET 200SP Manual Collection hope this helps, regards, |
FCK WAR! |
|
2/13/2017 9:49 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hi, Have a look to this: TIA Selection ToolThe TIA Selection Tool provides wizards for selecting individual devices and entire plants. It helps the user select modules and accessories, checks slot rules, and prevents errors during selection. The TIA Selection Tool generates a complete order list directly from the products selected or configured by the user. This list can be directly exported into the Industry Mall shopping cart or can be exported in a common standard format. Components that can be selected and configured include PLCs, distributed I/O systems, HMI panels, industrial PCs, drive systems, industrial controls, software, communications technology, power supplies, and industrial identification systems. Users can also create PROFIBUS and PROFINET networks, configure their topology, and select associated cables and connectors. hope this helps, regards, |
FCK WAR! |
|
Follow us on