Industry Online Support
Technical Forum
7/3/2013 7:15 AM | |
Posts: 262 Rating:
|
Hi, please check if we both are refereing to the below MLFB/ Type no 6ES7138-7FA00-0AB0. As i can see the data sheet, it accepts normal 0/4 to 20mA as an standatd input. Hence, you need to check maximum cable lenght and use a galvanometer/ multimeterto check if you are receiving the healthy signal. refer the attachement. AttachmentMzE3NzI3MTU5MjU2MTU0NzQzAAAA_46484943_2_inter_WW_2010-11-20.pdf (56 Downloads) |
7/3/2013 8:54 AM | |
Posts: 2 Rating:
|
Hi Valli, Yes that is the one my customer is using. Thanks for the clarification on it |
Follow us on