Industry Online Support
Technical Forum
6/9/2014 10:56 PM | |
Joined: 5/28/2008 Last visit: 5/28/2023 Posts: 4446 Rating:
|
I am not sure if it possible or not but it is not available in the attached "List of Modules" in the following FAQ: And attached you will found some possible configurations
AttachmentProduct Brief FM357-2 01_2003.pdf (27 Downloads) |
Last edited by: Ayman Elotaify at: 6/9/2014 11:13 PMAyman Elotaify |
|
This contribution was helpful to
1 thankful Users |
6/10/2014 1:08 AM | |
Posts: 17 Rating:
|
yes, it is not clear can or can't, in HW config of STEP7, is mention "6ES7 153-4BA00-0XB0 PROFINET IO device interface module IM 153-4 PN HF (ERTEC200) for S7-300 SMs, FM 350 to FM 352, FM 357, CP 340, CP341, CP343-2, PROFINET interface and 2 ports, FW update via bus; port diagnostics; I&M functionality; IRT and prioritized startup; MRP; firmware V3.0" and the doc"ET200 simatic_st70_chap09_english_2011.pdf" was not metion about FM357.
Attachmentet200m Specification.pdf (40 Downloads) |
Follow us on