Industry Online Support
Technical Forum
9/9/2014 12:13 PM | |
Posts: 2 Rating:
|
Hello, I'm trying to configure a ET200SP IM155-6PN ST (6ES7 155-6AU00-0BN0). I have installed that gsd file : gsd but when I open the catalog, it doesn't appear. I've tried to close and open TIA, to install it again but nothing changed. Any clue of what's happening? I'm using TIA portal V13 with step 7 pro The main CPU is a 1215C DC/DC/DC (6ES7 215-1AG40-0XB0) connected by profinet |
9/9/2014 12:34 PM | |
Posts: 1368 Rating:
|
Why do you installed GSD? The ET200SP is even integratedin TIA V13 hardware catalogue... Look under "Dezentral peripherie" > "ET200SP" |
9/9/2014 1:54 PM | |
Posts: 2 Rating:
|
I have ET 200S's installed but only IM 151-7, 151-8 and 154-8. not the 155-6. |
9/9/2014 2:34 PM | |
Posts: 1058 Rating:
|
Hello NedWR, actually Pittiplatsch is right, you should have it in TIA V13. But as I noticed, it came already with V11, so maybe your installation is not quite complete. But you can install via "Extras->Support packages" and then select "load from file system". The desired file you will find here: STEP 7 (TIA Portal) V11 Support Packages for the hardware catalog in the TIA Portal regards |
Follow us on