6/6/2010 12:56 PM | |
Joined: 2/26/2007 Last visit: 5/26/2023 Posts: 16 Rating:
|
Dear Friends, I am using IM151-8 CPU with DP master module,Modbus Module and DI/DO Modules.Here I have attached the program back. I find out the following points when I downloaded the hardware configuration to the CPU. 1. When I Configure the CPU and DP module alone in Hardware configuration of the Simatic Manager, The CPU in RUN mode and working fine. 2. If I add at least one or two DI/DO Module along with the CPU I am getting IO error. 3. Even I configured the DI/DO module, still the netpro view is showing only CPU and DP module. 4. The IP address of the CPU is not retaining. Please do the needful to come out from this problems.The attached program back up can be opened by usingSimatic Manager V5.4 SP4 or later versiononly.I have already confirmed that the power supply module is working fine. AttachmentNarans.zip (178 Downloads) |
Last edited by: aru at: 6/6/2010 12:57 PM |
|
Follow us on