12/5/2006 1:44 PM | |
Posts: 14 Rating: (0) |
Hello, Is it possible to use the ET200L and ET200s compact modules in PCS7V6.1SP1 wit regards Henri |
12/5/2006 3:50 PM | |
Posts: 1776 Rating: (95)
|
Hi Henri, i found this extract from PCS 7 V6. 1 SP1 readme (Its only for ET 200S); I found no information about ET200 2.1.9 New Signal Modules for ET 200M and ET 200S Preparations for using new signal modules have already occured for ET 200M and ET 200S stations. The integration occurs via "Hardware Support Packages" (HSP). The following modules for ET200M will only be released when the HSP "AI/AO 8x16Bit HART" (S7HSP0078) is released: 6ES7 331-7TF00-0AB0 6ES7 332-8TF00-0AB0 The following modules for ET200S are only released as replacement parts until the release of HSP "ET 200S SM" (S7HSP0093): 6ES7 131-4BB01-0AA0 6ES7 131-4BD01-0AA0 6ES7 131-4BB01-0AB0 6ES7 131-4BD01-0AB0 6ES7 132-4BB01-0AA0 6ES7 132-4BB31-0AA0 6ES7 132-4BB01-0AB0 6ES7 132-4BB31-0AB0 6ES7 132-4BD01-0AA0 6ES7 132-4BD31-0AA0 6ES7 132-4HB01-0AB0 6ES7 134-4FB01-0AB0 6ES7 134-4GB01-0AB0 6ES7 134-4GB11-0AB0 6ES7 135-4FB01-0AB0 6ES7 135-4GB01-0AB0 Please configure the previous module if you have not yet installed the HSP. The HSP will soon be provided on the PCS 7 Internet site under "A&D Service and Support". |
9/11/2007 7:40 PM | |
Posts: 1 Rating: (0) |
Hello ! Can I use an AO reference 135-4GB01-0AB0 in a project with PCS7 V7.0? Thanks. Jose Gil
|
9/11/2007 7:45 PM | |
Posts: 3149 Rating: (171)
|
Hi via search function I found this manual: http://support.automation.siemens.com/WW/view/en/24831707 nemo |