12/1/2015 3:24 PM | |
Posts: 111 Rating: (1) |
I have select the following Part number for ET200SP
I just want to make sure that do we need separate power module separately for this ET200SP or it is included in Interface module for the whole system as we do in ET200S? I also want to know the part number of Profinet Cable if somebody can provide me the part number of Profinet Cable for 10meters? Waiting for support. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/1/2015 4:02:48 PMNew subject after splitting |
|
12/2/2015 11:30 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi Shahjee, the ET200SP is different to the ET200s. You don´t need power-modules for establish new potential group. In ET200SP this is made by the Base-Units. See the manual collection of ET200SP chapter 3.4 of the first manual, page 38: SIMATIC ET 200SP Manual Collectionfor Profinet Cable have a look in the Industry Mall: Pre-assembled IE connecting cableshope this helps regards, |
Last edited by: mopS04 at: 12/2/2015 11:31:33 AMFCK WAR! |
|
This contribution was helpful to1 thankful Users |