Industry Online Support
Technical Forum
7/13/2009 11:09 AM | |
Joined: 1/17/2007 Last visit: 10/6/2020 Posts: 289 Rating: (3) |
Can I download/upload with laptop a H-Sysytem via ethernet CP443-1 instead of standard USB adapter? |
7/13/2009 11:32 AM | |
Posts: 76 Rating: (8) |
Yes, you must set the PG/PC interface to TCP/IP of your network card! |
7/13/2009 11:33 AM | |
Joined: 1/17/2007 Last visit: 10/6/2020 Posts: 289 Rating: (3) |
Thank you naah. |
7/13/2009 2:14 PM | |
Posts: 325 Rating: (14) |
Hi, Also check for IP address and subnet mask. Regards |
7/13/2009 4:12 PM | |
Posts: 49 Rating: (18) |
Hi, If its from standard LAN port, then you have to go with IE general connection.... Are u interested in communication with WinCC also.... Regards, Enigma |
7/13/2009 7:58 PM | |
Joined: 1/17/2007 Last visit: 10/6/2020 Posts: 289 Rating: (3) |
Thank you guys for support. I've established comm via laptop network adapter. |
Follow us on