11/27/2012 4:48 PM | |
Posts: 20 Rating:
|
I currently have two CPU 416-3 and i am trying to get comms between these 2 CPU's. I am trying to use FB209 and FB210. However the values are not being communicated and there is a error on the send blocks. can somebody please explain to me as there is no help file for these blocks. Is the ID the slot of the CP441-3 card on the CPU that the data is being sent from or sent to. And is there any other blocks or settings that i need to have in adition to the FB209 and FB210 blocks.
AttachmentHW Config.zip (56 Downloads) |
12/3/2012 12:31 PM | |
Posts: 3093 Rating:
|
Hello BillyBob, standard blocks have got "SIMATIC" or "SIEMENS" as Author. I don't know blocks with "COMM70" as author. Regards, Kaulquappe |
12/3/2012 2:05 PM | |
Posts: 20 Rating:
|
can you suggest what to use for this communiction then please |
12/3/2012 7:01 PM | |
Posts: 3093 Rating:
|
Hello BillyBob, the needed blocks depend on the protocol you are using. Just have a look at the compendium. Regards, Kaulquappe |
12/4/2012 10:08 AM | |
Posts: 20 Rating:
|
after looking at the compendiam i realised that the connection in the NetPro was not set to a active connection. Thank you and appriciate your time and advice |
Follow us on