2/10/2016 2:58 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, I would try it with Open Communication Blocks. T_CON for establish a connection T_SEND for Sending Data T_RCV for Receiving Data Here you find a FAQ and Application Sample: How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the ISO-on-TCP protocol for data exchange via the integrated PROFINET interface of an S7-300/S7-400 CPU or via the CP443-1 Advanced?hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to
1 thankful Users |
2/10/2016 3:12 PM | |
Joined: 10/1/2013 Last visit: 3/21/2025 Posts: 605 Rating:
|
Hi, using AG blocks is fine. For further information about the AG blocks and projected connection via NetPRO check out these FAQs: |
Last edited by: Owei at: 2/10/2016 3:22:07 PMLast edited by: Owei at: 2/10/2016 3:39:02 PM |
|
2/10/2016 4:29 PM | |
Posts: 3093 Rating:
|
Which protocol do you use? Ethernet is just the physics... Regards, |
Follow us on