12/17/2012 3:00 PM | |
Posts: 3093 Rating:
|
Hello GVT, which protocol do you use? Regards, Kaulquappe |
12/17/2012 3:08 PM | |
Posts: 15 Rating:
|
I use TCP/IP which means TSEND_C and TRCV_C. Thank you Best regards |
12/17/2012 4:56 PM | |
Posts: 3093 Rating:
|
Hello GVT, have you got a manual for the communication of the converter? Regards, Kaulquappe |
12/18/2012 8:07 AM | |
Posts: 15 Rating:
|
Yes, I have. Here is web page. http://www.dv-mir.ru/katalog/M_F5_M_2_7_eng.pdf Best regards
|
12/18/2012 12:15 PM | |
Posts: 15 Rating:
|
Hello. Keb wrote me, that they use protocol calledDIN66019II. Can somebody this protocol? Thank you Best regards |
12/18/2012 3:47 PM | |
Joined: 9/27/2006 Last visit: 3/19/2025 Posts: 12344 Rating:
|
Hello GVT, guys; According to this document from KEB, DIN 66019-ii corresponds to Modbus TCP: http://www.keb.de/fr/produits/technique-de-commande/combicontrol-c6/embedded-control.html Can anyone else confirm this, based on this description of the KEB DIN66019-ii standard: Entwicklungsinformation Development Information If it is correct (or oif KEB can vouch for it) then Siemens does offer a connection to Modbus/TCP: S7 OpenModbus/TCP - IT4Industry - Siemens |
Follow us on