3/1/2016 10:27 AM | |
Joined: 7/1/2013 Last visit: 1/22/2025 Posts: 85 Rating:
|
I am trying to establish communication between ET200S IM151-8 CPU (profinet interface) and CPU 312 (mpi interface). There is eWon as gateway (or protocol converter). In attached picture "HMI_Routed" you can see connection between PLC_2 and PC_System_1 which is working. That connection is created atutomattically by TIA portal when I add tag from PLC_2 to PC_System_1 tag table. I am unable to make this connection manually. On attached picture "PLC_to_PLC_error" faulty connection between PLC_4 and PLC_2 can be seen, which prevents hardware configuration compilation. Is this possible to be done in TIA, how can I create ruouted connection manually ? Best Regards AttachmentROUTING.zip (155 Downloads) |
Follow us on