8/7/2017 10:26 AM | |
Posts: 59 Rating: (0) |
Dear Sir, I am trying to use direct HMI Simatic Cmfort Outdoor TP1500 (without any external controller dedicated to the HMI) with multiple Logo!8 controllers to monitor & control process of the Logo controllers. For data transfer mapping at Logosoft Logo to HMI connection (logo client and HMI server), provision for logo tag addresses are configurable but for HMI, HMI tag (editable) and data type ( selectable from 1 to 99) are not easily configurable (showing remote address not valid). Please help me for the above issue with an example project. . ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/7/2017 10:59:26 AMNew subject after splitting Last edited by: fiah at: 8/7/2017 11:48:22 AMLast edited by: fiah at: 8/7/2017 11:51:37 AM |
|
8/15/2017 11:10 AM | |
Posts: 59 Rating: (0) |
I have successfully done the project.. |