Industry Online Support
Technical Forum
2/22/2010 5:06 PM | |
Posts: 21 Rating:
|
Hi Everybody, I did theexample that show the exchange data between CM1241_RS232 and Hyper terminal and one screen in the KTP600PN. The logic is not complicated...only 2 blocks like SEND_PtP and RCV_PtP is necessary. Enjoy it! AttachmentRS232_PtP.zip (1348 Downloads) |
3/4/2010 2:53 PM | |
Joined: 5/28/2008 Last visit: 5/17/2022 Posts: 1343 Rating:
|
Without having a look to the program i would say there is a problem with start address of RX buffer. Please have a look here at the 8th reply: https://www.automation.siemens.com/tf/WW/en/Posts/39432 There is also an application online, that desribes the PtP-Communciation: Flexible Decoding and Processing of Data Matrix Codes with S7-1200 (CE-X27) |
Follow us on