6/3/2011 8:40 PM | |
Joined: 12/20/2008 Last visit: 6/25/2024 Posts: 556 Rating:
|
I am attaching one attachment of errors which I got when I open the hardware configuration. After that I upgraded my hardware configuration and still got few errors which is attached in second attachment. I have tried almost everything by researching this forum, but still the problem has not been resolved. I just want to avoid uninstalling / Installing of Simatic manager. Please advise, by looking at the two attachments. AttachmentSiemens STEP 7Error.zip (157 Downloads) |
Last edited by: Lucky123 at: 6/3/2011 8:42 PMUploaded both attachments in zip format |
|
6/4/2011 3:11 AM | |
Posts: 691 Rating:
|
Dear Please install Step 7 V5.5 for opening your project. The CPU MLFB number is suppoterd in STEP 7 V5.5 AttachmentSiemens STEP 7Error1.pdf (138 Downloads) |
6/4/2011 6:21 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Hello, Please tellus the MLFB of your CPU 317-2 PN/DP.Have a look at the attached file and confirm that particular MLFB is available in your Hardware Catalog. As you Can See attached file is from Step7 V5.4 SP5. i don't think that you require to install Step7 V5.5. Have a look at this link. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=6ES73172EK140AB0&caller=view The latest CPU MLFB is 6ES7317-2EK14-0AB0 CPU317-2 PN/DP, 1 MB . which is available in Step7 V5.4 Sp5 |
Last edited by: Amit_86 at: 6/4/2011 6:22 AMVANDE MATARAM..... |
|
6/4/2011 7:04 AM | |
Joined: 2/6/2009 Last visit: 6/18/2024 Posts: 939 Rating:
|
Hi Amit, I think shar is correct, because the error as shown in the Luck's attachement the error says that the Step7 is not compatable. So he has install the Step 7 V5.5. and try that. Please have a look into the attachment and I have highlighted the error about step 7 version.
AttachmentSiemens STEP 7Error1.pdf (107 Downloads) |
_______________________________________________________________ |
|
6/4/2011 7:18 AM | |
Joined: 12/20/2008 Last visit: 6/25/2024 Posts: 556 Rating:
|
Hi Amit, I think shar is correct, because the error as shown in the Luck's attachement the error says that the Step7 is not compatable. So he has install the Step 7 V5.5. and try that. Please have a look into the attachment and I have highlighted the error about step 7 version. I had step7 v5.4 sp5 in my old laptop, in which project was developed, so i m sure its not because of version issue.
|
6/4/2011 7:22 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
I had step7 v5.4 sp5 in my old laptop, in which project was developed, so i m sure its not because of version issue. Hello Lucky123, i am 100% agree with you.you don't need to install Step7 V5.5. Please Provide MLFB of your CPU if possible. |
VANDE MATARAM..... |
|
Follow us on