6/11/2017 6:55 AM | |
Posts: 9 Rating:
|
Hi, I downloaded document & Program file from the below link of application example. https://support.industry.siemens.com/cs/ww/en/view/67261457 In the HMI Tag I found an address that is "DB [DBNr] DBX [offset_byte1].0" but i can't understand which DB & Byte is defined of PLC program by this HMI Tag. Please explain the meaning of this HMI Tag. Find the attached file for your better understand. ------------------------------------------------------------------------------------------ |
Last edited by: Mustafez at: 6/11/2017 6:57:28 AMLast edited by: Min_Moderator at: 6/12/2017 2:22:07 PMNew subject after splitting |
|
6/12/2017 1:35 PM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello here it is described how it works: How does adress-Multiplexing work: https://support.industry.siemens.com/cs/ww/en/view/21808320 Bye Murof |
If this Information really helps, you could use the Rate function |
|
6/13/2017 11:22 AM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello together So, first to prevent missunderstandings there are two ways of using Multiplexing in WinCC flexible (as we can see in the Screenshot of Mustafez) Tag Multiplexing: https://support.industry.siemens.com/cs/ww/en/view/21807421 Adress Multiplexing: https://support.industry.siemens.com/cs/ww/en/view/21808320 The Adress Multiplexing is a coplete indirect adressing as Mustafez uses in his project. In this 2 FAQ is everything explained you have to know. I do not understand the last post of User zzVss????? Please zzVss read first the FAQs an then write again Bye Murof |
Last edited by: Murof at: 6/13/2017 11:22:53 AMLast edited by: Murof at: 6/13/2017 11:23:36 AMIf this Information really helps, you could use the Rate function |
|
6/13/2017 12:55 PM | |
Joined: 5/30/2013 Last visit: 3/24/2025 Posts: 112 Rating:
|
Hi Murof, the 1st image show (when opened) program that the HMI tag don't use multiplexing. the 2nd image show when HMI tag used in multiplexing (this the picture we will see in FAQ How does tag multiplexing work image3). I try have explained very simple haw in this case (this project) used fix HMI tag by different value. In the project you have seen haw this working (see image): For better understand tag e.g. (in the project) ActPackAxis [bool] => DB [DBNr]. DBX[offset_byte7].7 DBNr depending of logic operation (PLC) will be 72 (Int)-> DB72 or 172 (Int)->DB172. offset_byte7 (Internal tag--Int ) depending of operation in panel (Cross_Reference for offset_byte7) Best regards zzVss |
Follow us on