5/26/2009 4:36 PM | |
Posts: 99 Rating: (7) |
Hi is there anyone who knows how i can make an export of te values from taglogging to a csv fileat once. first i tried it with a c script and the help from ODK (Open development kid) see my topic /tf/WW/en/Posts/29908#top now i have conectivity pack and can reech the data base. But i have to tell in the script of which tags the values has to be exported. It is possible, but i thought it must be possible to make an export of the database in one time. Is there anyone who knows of this is possible or not. Thank for thinking |
6/3/2009 10:37 AM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
hi the easiest way to export taglogging datas is to use the export function of the table control or the trend control. There you can define many filters too. regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
6/3/2009 2:35 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
hi i understand. here is samthing like you want, maybe it helps. http://support.automation.siemens.com/WW/view/en/26697936 regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
6/3/2009 4:06 PM | |
Posts: 150 Rating: (2) |
Regarding the export function on the trend control window, do you now why miliseconds are not shown in the cvs file?? |
Follow us on