Industry Online Support
Technical Forum
12/7/2009 8:17 AM | |
Joined: 9/29/2005 Last visit: 12/16/2024 Posts: 313 Rating:
|
Hi, the Micro Automation Set 21 generates automatical the *.csv-file from a script in WinCC flexible which is the OPC-client. So you can have a look to the WinCC flexible project and navigate to the "Scripts". (See chapter 3.7 in the documentation "Micro Application Example") I have no idea how you can export those OPC-stored data directly into a *.mdb or *.csv-file or *.whatever without WinCC flexible. regards |
Last edited by: Lifrasil at: 12/7/2009 8:24 AM |
|
This contribution was helpful to
1 thankful Users |
Follow us on