3/12/2018 11:01 AM | |
Posts: 1 Rating:
|
Dear Experts, please help me, The question is whether it is possible to simultaneously supply the FSGX drive with an external 24 V supply to the control unit (terminals T31, T32) and to the terminal block X9 PM240 (T1, T2). 400 V is supplied through the line contactor permanently. I have a non-periodic error F30022. AttachmentSINAMICS G120 Connecting external DC 24V power supply.pdf (46 Downloads) |
Follow us on