3/20/2017 1:26 PM | |
Posts: 9 Rating:
|
Hi guys, I am confused about total current consumption of safety output module 6ES7226-6DA32-0XB0 . In datasheet it is current consumption defined as follows: - from backplane bus 5 V DC, max. 125 mA, - from load voltage L+, max. 170 mA so total input current is 295 mA but output current for signal "1" rated value is 2 A. The module has 4 DQ so total output current for "1" is 8A ? I think input and output currents should be the same. Am i wrong? |
Follow us on