4/27/2012 5:10 PM | |
Posts: 557 Rating:
|
Hello, I am using F-Switch afterward 2 DO'S, in that case if F-Switch disable the bus then output will off or not? If I use F-switch afterword 2 DO's module then again F-Switch then afterword 1 DO module, in this case if my first F-switch disable the bus, in that case my output module which is connected to next F-switch will work or not? Regards |
4/28/2012 11:11 AM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, In the ET200 Pro failsafe modules manual http://support.automation.siemens.com/WW/view/en/22098524 - at page 129 you see the assignments of the outputs of the F-switch - at page 130, you have a drawing showing how the F-switch acts for digital outputs. There is an entry with a list of modules that you can plug behind an F-Switch http://support.automation.siemens.com/WW/view/en/25371449 In my opinion, if you want to putmore than oneF-switches in a ET200Pro, you must also add for each additional F-Switcha new power moduleP-ME before the F-switch (to start a new potential group). |
Best regards |
|
This contribution was helpful to
2 thankful Users |
We are working on a new user interface with better overview and more relevance.
Follow us on