2/20/2021 2:06 PM | |
Joined: 12/6/2016 Last visit: 11/14/2023 Posts: 76 Rating:
|
1/ its the value read by the control unit and i watch it in starter with drive navigator menu. I'll check this with an ammeter. 3/ this is motor data: [snip] i tell more things; a/ when we were testing different setpoints and speed motor, we have to drecrease slip compensation until 10% (p1335) because the motor rotates more quick that setpoint (+-50rpm) tested with a tachometer. b/ we have 1300=0, may be better with another mode of u/f or....even in vector control encoderless. c/ i think the problem can be too, that the motor haven't any load and not installed brake resistor, by the moment... Thank you very much!! |
Last edited by: Jen_Moderator at: 02/22/2021 08:42:08Removed link and added file as an attachment. |
|
This contribution was helpful to
1 thankful Users |
Follow us on