3/17/2019 5:08 PM | |
Joined: 9/24/2013 Last visit: 4/15/2025 Posts: 36 Rating:
|
Hello. Thanks for a reply. The communication load due to program cicle i will test that . The data is stored inside the DB's withoud optimalization inside the PLC. There's no other than HMI writting on this data . The data is used by the FB operating the part of the line, there's no write operation only read and use as a parameter for the timers. I add the screeenshots of the configuration of the project . It's simple configuration done for small test mashine . AttachmentS7 screens.zip (117 Downloads) |
Follow us on