7/20/2023 9:22 AM | |
Joined: 7/6/2023 Last visit: 7/26/2023 Posts: 3 Rating:
|
Hi all, I am using WinCC Unified v18 and I have an issue with my faceplates getting erased when I'm moving inside a screen window. I am trying to display the layout of a plant in a screen bigger than the screen window container with the ability for the user to move around and zoom in and out. When the zoom factor is 1 everything works fine but if I'm zoomed in or out, items start to disappear near the edges and as far as the middle of the screen when I navigate to the left end side of the screen. The only items erased this way are the faceplate containers. I have tried looking into both the screen and the faceplates minimum and maximum zoom factor but the issue doesn't seem to come from that. I have attached a short video showcasing that I described. I would be very grateful for anyone having a solution. Attachment2023-07-20 11-12-03.mov (21 Downloads) |
7/20/2023 9:34 AM | |
Joined: 1/21/2013 Last visit: 10/1/2023 Posts: 2084 Rating:
|
Hi, I am missing some information about your device. However, in case of a Unified Comfort Panel, your number of faceplates may be too high, as a maximum of 40 should be used. You should check if the latest update is installed (to provide a download link I would need to know if you are using a panel or the PC runtime). If the behavior does not change then you should contact Siemens and create a support request. Kind regards |
7/20/2023 10:38 AM | |
Joined: 1/21/2013 Last visit: 10/1/2023 Posts: 2084 Rating:
|
Hi, So in addition to creating a support request, I would suggest that you install:
Kind regards |
7/20/2023 1:13 PM | |
Joined: 7/6/2023 Last visit: 7/26/2023 Posts: 3 Rating:
|
Updating WinCC Unified PC Runtimed solved the issue, thank you for your help ! |
Follow us on