9/29/2016 10:27 AM | |
Joined: 9/15/2014 Last visit: 5/4/2022 Posts: 2 Rating:
|
Dear All, I've a system which I wanted to integrate with an OPC Scout server (Simatic Net V13 Sp1). I did the configuration & communication is showing ok in station configuration, but when I'm compiling it after configuring tags as shown in config image it is generating two erros also attached. I am unable to understand what period it is mentioning. Can someone explain. I need support on urgent basis. Thanks & Regards, Deepak AttachmentConfig.zip (53 Downloads) |
Follow us on