6/28/2021 4:20 PM | |
Joined: 12/12/2016 Last visit: 9/29/2023 Posts: 640 Rating:
|
Hello, If you can still boot into the IndustrialOS, you could copy the attached config file into /etc and then use the command
In order to change the boot priority. Elsewise you would most likely need a FTDI Cable. Indeed the Example Image available on SIOS is currently still the (old) V1.0.2, I would recommend to build a fresh one with the current master branch. BR Attachmentfw_env.zip (141 Downloads) |
7/21/2021 3:21 PM | |
Joined: 10/19/2019 Last visit: 6/16/2022 Posts: 2 Rating:
|
Hello everybody, How do I copy the attached file?
|
Follow us on