Industry Online Support
Technical Forum
6/21/2013 8:04 PM | |
Posts: 88 Rating: (0) |
Thanx for your reply... according to you I have to download and install applications in my ES, which is not possible for me...pls give other suggestions..... |
6/29/2013 10:39 PM | |
Posts: 62 Rating: (4) |
Dear Friend, event > Failure connection ID 0 Source > S7 program(AS1) /@(5) / AI8X12bit_5 event > module error0/0/0 Error channel 00 Source > S7 program(AS1) /@(5) / AI8X12bit_5 event > module error0/0/0 Error channel 04 Source > S7 program(AS1) /@(5) / AI8X12bit_5 event > module error0/0/0 Error channel 05 There is a specific Reason for grtting this Kind of Massages. event > Failure connection ID 0 this Means that this error occer due toS7 program(AS1) /@(2) / AS1_(IC9301). if u go to this folder u can find why this error occer. These Errors Are Sysyem Generated u will find this in @ Charts in the Chart Folder. Regards, AvinashKrishna Bhimavarapu.
AttachmentCpu Generated Blocks.zip (241 Downloads) |
7/10/2013 8:10 AM | |
Posts: 88 Rating: (0) |
Despite of above alarm the following alarms came with priority 0. 1) SCRIPT:XXINAS120S:Action-Error 2) PDLRT:XXINAS120S:Picture not found |
7/10/2013 9:29 AM | |
Posts: 88 Rating: (0) |
Thanx Avinash! as per your procedure I opened the chart@9. but there I found only CPU_1 is configured. But in my case now CPU_2 is in MASTER and not configured any where in chart. The alarm ID failure also come for CPU_2. so pls help for eliminate the problem. regards, |
Follow us on