5/16/2007 1:58 PM | |
Posts: 3149 Rating:
|
Hi have you seen this? http://support.automation.siemens.com/WW/view/en/12836439 http://support.automation.siemens.com/WW/view/en/20712944 nemo |
5/16/2007 2:01 PM | |
Posts: 1084 Rating:
|
Question: is SIMATIC Rack PC IL 40 S V2 PSC7 then? with regards, Ikkezelf |
5/16/2007 2:18 PM | |
Posts: 75 Rating:
|
SIMATIC Rack PC IL 40 S V2 with WinCC6SP4HF2 (not PCS7). |
5/16/2007 2:28 PM | |
Posts: 75 Rating:
|
What version of the driver needs to be used with WinCC6SP4HF2? |
5/16/2007 2:39 PM | |
Posts: 1275 Rating:
|
Here's something I found under this link, for technical support on the product: Technical Support / Hotline You can get support for the Multi-VGA graphics card from the Technical Support (Hotline) of Automation and Drives. Information on our central Technical Support, as well as addresses with fax and e-mail data is available from the Internet Site of "Automation and Drives, Service & Support" under "Services -> Technical Support". For more information please get in touch with your SIMATIC contact at your local Siemens office. Ikkezelf mentioned something interesting: check the IRQ for the board, and see if it's a suitable one. You could also just try re-installing the device. The installation of other devices after this one may have caused it to switch IRQ, or something else... and if that's the case, re-installing may do the trick. Best regards, Danielle |
Follow us on