9/25/2020 3:26 PM | |
Joined: 10/24/2011 Last visit: 6/4/2024 Posts: 4 Rating: (0) |
Hello everyone, I have a similar situation : no Profinet communication between PLC and robot. -robot Fanuc R-30iA -CP1604 v2.5, A05B-2500-J930 v2.5 mainboard A05B-2500-J930 -GSDML: GSDML-V2.25-Fanuc-J930-20120113.xml installed -PLC : S7-300 319F-3 PN/DP v3.2 -switch: SCALANCE X216 16 ports. The PING command to the IP of the robot works ,but the robot show up as offline in the online hardware config page. I am using Simatic Manager Step 7 V5.6 + SP2. Any thoughts on this? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 09/25/2020 16:01:57New subject after splitting |
|
4/21/2021 7:31 AM | |
Posts: 1 Rating: (0) |
你好.我需要这个gsdml文件,方便给我一下吗?我们也有几台发那科R30iA的机器人,想试一下 |
4/21/2021 11:11 AM | |
Joined: 6/19/2017 Last visit: 6/11/2024 Posts: 8165 Rating: (165) |
Hi Jimmyhuhuhu, Please, try to discuss your question in English language. This is an international community and we try to focus on one language. Posting in English will help you to get more response to your question. This is the translation of your question:
Best regards, |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to2 thankful Users |
4/23/2021 11:44 AM | |
Joined: 3/9/2018 Last visit: 5/24/2024 Posts: 5 Rating: (1) |
Dear, Is this an CP1604 card or an CP1616 card or a Molex card? |
10/31/2021 11:12 AM | |
Joined: 12/16/2020 Last visit: 5/27/2024 Posts: 2 Rating: (0) |
Did you got this gsdml? .. i am also searching for it. If possible with a example to use it in TIA. Thnx. |
Follow us on