12/18/2019 6:55 AM | |
Posts: 2 Rating: (0) |
Hi guys I have a question Can i use fast inputs at the same time in LOGO ? ...sent from App |
12/18/2019 9:20 AM | |
Posts: 2 Rating: (0) |
yes, i want use two input at the same time for counting. thanks for answer |
12/18/2019 8:04 PM | |
Joined: 12/27/2006 Last visit: 11/29/2024 Posts: 1197 Rating: (113) |
Yes, thats possible, but you must have 2 counters. Or make a total of 2 counters. Look at the attachment. You must use the right LOGO and the right inputs, the programm is only to demonstate how you can count 2 (or more) counters. AttachmentTotalCount.zip (225 Downloads) |
Follow us on