4/12/2018 8:14 PM | |
Joined: 6/4/2010 Last visit: 2/11/2025 Posts: 35 Rating:
|
I have to install to a Profibus network a DP / DP coupler. In this network, there are three "Terminal Bus". I installed this DP / DP on the network between the termimal bus 1 and 2. After that, it does not work. I have a communication fault. You will probably ask me if the configuration of the DP / DP is correct. The addressing is correct. Note that the fault is at the entrance. At the exit to the other PLC, I have no mistakes. Also, when I make a compilation, I have no errors. I send you a file that shows how the network is doing. What do you advise me to make everything work normally? AttachmentRéseau Profibus des Turbodrains.xlsx (103 Downloads) |
Last edited by: ElectroTCC at: 4/12/2018 8:15:09 PMLast edited by: ElectroTCC at: 4/12/2018 8:17:42 PMLast edited by: Jen_Moderator at: 4/13/2018 11:08:58 AMEdited text for better reading. Dany Thibeault |
|
4/12/2018 8:32 PM | |
Joined: 6/4/2010 Last visit: 2/11/2025 Posts: 35 Rating:
|
Here is an overview of the two Profibus networks. |
Dany Thibeault |
|
Follow us on