7/26/2017 11:36 AM | |
Joined: 5/12/2006 Last visit: 6/5/2024 Posts: 22254 Rating: (2986)
|
Hello, attach the messages! Also check if any fault active after the download, attach a screenof it |
7/27/2017 10:23 AM | |
Posts: 22 Rating: (0) |
when i download from starter to CU310-2DP : |
7/27/2017 10:24 AM | |
Posts: 22 Rating: (0) |
and sinmic Fault F7080 |
7/27/2017 10:43 AM | |
Posts: 22 Rating: (0) |
all fault |
7/27/2017 10:58 AM | |
Posts: 22 Rating: (0) |
yes i fix p346=2 and sinamic Fault F07080 anh alarm: |
7/27/2017 11:09 AM | |
Joined: 5/12/2006 Last visit: 6/5/2024 Posts: 22254 Rating: (2986)
|
which value have the alarm 7080 ? This value represent a wron parameter , you should check this parameter |
7/27/2017 1:34 PM | |
Posts: 22 Rating: (0) |
Thank all expert! i can do it |
Follow us on