Industry Online Support
Technical Forum
8/9/2012 10:08 AM | |
Posts: 44 Rating: (6) |
Hello! Does the drive boot without memory card? Dit you read operating instruction, chapter 9.1.4 ? Poweringon the drive with a plugged in original memory card starts a firmware update. Did you see the status of the LEDs? Please compare with chapter 10.30.4 of operation instruction. If the drive is booting withot memory card --> OK You can try again a firmware update (power up with plugged in memory card). Have a lookat the status of the LEDs during firmware update. Don´t switch off during update!!!! If it´s working --> OK If you still have problems --> probably you have destroyed the boot sector of TMS320 controler. In that case please change CUD. Boot sector can be repaired in the factory. Link to the operating instructions: http://support.automation.siemens.com/WW/view/en/59381290 regards frimos |
10/16/2012 6:54 PM | |
Posts: 44 Rating: (6) |
Update firmware in the CUD: http://support.automation.siemens.com/WW/view/en/44029688 |
6/10/2016 1:42 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by Alfa2010 is split to a separate thread with the subject Sinamics DCM 6RA8075 problem. Best regards |
Follow us on