6/26/2013 7:50 AM | |
Joined: 11/18/2010 Last visit: 8/5/2022 Posts: 523 Rating:
|
ya but acceleration setting is also is same important as torque limit please set as practical requirement |
6/27/2013 7:57 PM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating:
|
I am agree with zako_'s reply Most chances are improper encoder signal. Increase in torque limit should be done only afterbeing double sure about it Regards, Devesh |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
7/1/2018 5:32 PM | |
Joined: 6/25/2018 Last visit: 8/9/2021 Posts: 1 Rating:
|
dear sir SIMOTION ERROR IS COMMING 7900 |
12/20/2019 4:11 PM | |
Posts: 1 Rating:
|
A wiring problem on the drive can cause this fault. Check wires U2 V2 and W2 |
Follow us on