5/26/2015 12:29 PM | |
Joined: 10/3/2013 Last visit: 9/14/2024 Posts: 125 Rating:
|
Hi, I also have some doubt, kindly refer attached picture; Picture 1- HWD 400H: It shows hardware configuration of 400H with two Profinet IO systems with different subnets. It complies without error. Picture 2- Netpro 400H: Same project in Netpro,; compiles with error (Picture 3- Error Massage). If both Profinet IO system-1 & Profinet IO system -2 are connected to the same subnet then only it compiles in Netpro. (Picture-4). If have to set fault tolerant connection between PC station & 400H with Profinet IO System; the hardware configuration shown in Picture-5; But is shows the same error message shown in Picture-5. & With same subnet it does not shown error. (Picture- 6) That means, Can fault tolerant connection between PC station & 400H not possible with different subnet?
----------------------------------------------------------------------------------------------------
Attachmentpictures.docx (116 Downloads) |
Last edited by: Min_Moderator at: 5/27/2015 1:37:32 PMNew subject after splitting |
|
Follow us on