10/8/2014 11:01 AM | |
Joined: 4/24/2006 Last visit: 3/21/2025 Posts: 8904 Rating:
|
Hello Fani.lng, Please have a look at the followinglink: how do you program communication blocks FC11 and FC12 for the PROFINET IO controller? The problem is caused by the amount of bytes you want to read and write. See the addresses of IO device, when you use addresses 260 etc. (You should at least communicate more then 260 bytes, even when you do not use the first bytes) Try to change the addresses to a lower address, so you can communicate less bytes Best regards, Wizard |
10/8/2014 2:07 PM | |
Posts: 77 Rating:
|
Hello, I have done that according to 283 and 282bytes size.
|
10/8/2014 2:24 PM | |
Posts: 77 Rating:
|
I attached a picture of data block and the code. |
This contribution was helpful to
1 thankful Users |
Follow us on