12/17/2009 2:26 PM | |
Joined: 12/9/2009 Last visit: 4/18/2024 Posts: 156 Rating:
|
Hello, the code 80B1 means: "Destination area is invalid. The amount of data to be sent exceeds the upper limit permitted for this service (e.g. destination area > 240 bytes)." But when I look to your calls of FC5 and FC6 the the destination area seems ok.Strange Do you have already tried to use a DB as send and receive buffer??? Or try the following sample programs. May it works. FC50 and FC60 for S7-400: http://support.automation.siemens.com/WW/view/en/24693800 FC5 and FC6 for S7-300: http://support.automation.siemens.com/WW/view/en/24675522 In thesample programsan error logging is implemented. |
1/4/2010 8:31 AM | |
Joined: 5/6/2008 Last visit: 2/11/2025 Posts: 57 Rating:
|
Dear all: AttachmentArchive.zip (370 Downloads) |
4/30/2015 3:37 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating:
|
|
Follow us on