12/6/2024 8:50 AM | |
Joined: 12/6/2024 Last visit: 3/9/2025 Posts: 2 Rating:
|
Am getting the error in HMI for example the button is for feed pump, in HMI while pressing the button its showing like feed pump value cannot be written to the PLC. Am using TIA 19 and HMI comfort panel TP1500, please help me with this issue as soon as possible ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 12/06/2024 09:12:11New subject after splitting |
|
12/6/2024 3:16 PM | |
Joined: 4/24/2006 Last visit: 4/18/2025 Posts: 8956 Rating:
|
Hello, Perhaps you can give some more information? (Version of CPU, HMI etc.) The following links might help: No connection to PLC after WinCC Panel Images V17 Update 6 Check the date and time of HMI. or Configure an HMI connection to an S7-1500 CPU with FW V3.1 Best regards, Wizard |
12/12/2024 9:21 AM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello Still Viz So do other signals work in simulation? perhaps you have no connection to your PLC or PLCSim? check this basic FAQ: https://support.industry.siemens.com/cs/de/en/view/109748099 perhaps only the PGPC Interfaces settings are not set properly or something like this Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on