4/14/2016 12:58 PM | |
Posts: 160 Rating:
|
Hi, things didn't go as I expected... I'm having some trouble configuring FW_TCP fb... 1. I'm no sure that I'm calling it correctly (PIC 1). It this enough? Did i miss something? 2. What should CONNECT pointer type Any has to point to the where? From help: "ANY pointer to the data area of DB211 that contains the parameters for establishing the TCP connection. This data area must be at least 64 bytes in size.". To be honest I didn't understand a thing... (PIC 2) 3. This might be related to the 2. but where do I specify which data FW_TCP should read and where to write fetched data? If you have any kind of a working example, it should be of a great help. Anyway, thank you all in advance! Best regards, Janko PIC 1/2 in DOC file. AttachmentDOC.pdf (363 Downloads) |
Follow us on