5/4/2010 7:40 AM | |
Joined: 8/22/2009 Last visit: 6/5/2023 Posts: 41 Rating:
|
with HMI (Shneider Electric) and siemens s5.we use fetch and write service as in this link [c Fetch and write service] my question can i use fetch and write service work on TCP Native and at the same time of using profinet IO . i have to use schneider HMI this is the problem and i also have et200s the link explain how to implement Fetch and write service on integerated profinet port of s7. so can i use profinet io too from the same port for et200s i used hardware configuration and used these FB for fetch service and also Et200s there are no problems appeared? |
Veolia |
|
5/5/2010 7:31 AM | |
Joined: 8/22/2009 Last visit: 6/5/2023 Posts: 41 Rating:
|
WAITING FOR YOUR HELP |
Veolia |
|
5/5/2010 5:04 PM | |
Posts: 5822 Rating:
|
Dear Ahmed, I would say the answer is yes. Best regards J_Bell |
Follow us on