5/24/2022 8:03 AM | |
Joined: 6/11/2018 Last visit: 4/5/2024 Posts: 27 Rating:
|
Hello to everyone, i want to make a programm that a button start fills the tank which when I throw it will arm the relay at the output (the relay is 24vdc) and the green light will turn on, ie run that it fills! The stop will simply close the intake valve and will not put any more water! Then with a 0-1 switch the exhaust valve will open, ie the tank will be empty! Then with a switch 1-0-2 it will become automatic / manual (if the switch 1-0-2 is not convenient I put a black button) and the orange light will light up when it is in automatic! In automatic mode I would ideally like when the tank is below 30% to turn on the red light which will mean that the tank is empty, and put water until it reaches 80% Attachmentfilllevel 30_.zip (443 Downloads) |
Last edited by: Dimsenio at: 05/24/2022 08:05:13Last edited by: Dimsenio at: 05/24/2022 08:51:56 |
|
5/24/2022 11:13 AM | |
Joined: 6/11/2018 Last visit: 4/5/2024 Posts: 27 Rating:
|
I make a program it works but with float level switch 30% and 80 % , i want to make the same solution but with analog control with sensor pressure 0-300cm , 4-20 mA , 0-12 bar. Attachmentfilllevel_SWITCH 30_80_%EN.zip (454 Downloads) |
5/24/2022 1:13 PM | |
Joined: 12/18/2014 Last visit: 7/27/2024 Posts: 33421 Rating:
|
Try this.
Attachmentfilllevel_SWITCH 30_80_%EN_V2.zip (504 Downloads) |
This contribution was helpful to
1 thankful Users |
5/24/2022 10:32 PM | |
Joined: 6/11/2018 Last visit: 4/5/2024 Posts: 27 Rating:
|
It was my mistake the cable from I6 to and B009 not need! now is completely correct Ixo thank you very much for your help! Attachmentfilllevel_SWITCH 30_80_%PRESSURE_V3.zip (502 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on