7/6/2013 2:52 PM | |
Posts: 8946 Rating: (999) |
Siemens will be happy to explain you.... |
This contribution was helpful to1 thankful Users |
7/6/2013 2:59 PM | |
Joined: 1/20/2008 Last visit: 9/14/2024 Posts: 120 Rating: (7) |
|
7/6/2013 4:41 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello, Just to add some comments beside what has been mentioned yet.We have not the source project of the firmware with all details inside.But, We read manuals and material about behavior of S7300 /S7 400 CPUs.The instructions how to handle downloading, restart behavior, interrupt handling and program execution are instructions derived based on the firmware of CPU. All we need are available in "Manuals" and "Books" and that suffice us.Finally the whole instruction set that is also a characteristics of the main processor.I also suggest checking the following topic for a better understanding: [?] What is the architecture of S7 CPU's?CPU 315-2 PN/DP PROCESSORHope that helps Hamid Hosseini |
Last edited by: hdhosseini at: 7/6/2013 9:28 PM |
|
Follow us on