10/7/2020 10:56 AM | |
Joined: 3/30/2020 Last visit: 4/25/2025 Posts: 5084 Rating:
|
An installation of WinCC V15.1 is needed. The good news is that V15.0 and V15.1 can both be installed. These also use the same license. The exception is WinCC Professional -- there can only be one installed WinCC Professional. You can use the trial version as source of the software. The base version V15.1: The latest update for the base is update 5: This problem now solved? |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
1 thankful Users |
10/7/2020 11:24 AM | |
Joined: 2/10/2016 Last visit: 3/27/2025 Posts: 118 Rating:
|
Thanks qwazze its clear now for me.all options are available |
This contribution was helpful to
1 thankful Users |
Follow us on