Industry Online Support
Technical Forum
4/29/2014 3:22 PM | |
Joined: 12/15/2010 Last visit: 5/30/2014 Posts: 13 Rating: (0) |
The flow range is wide and will depend of the pipe size; in our catalog FI 01 2014 page 3/25 & 3/16 we have a flow table that applies as a reference for this particular need.Additionally, for thecustody transfer version, we have aclearly definedrange of flow based in the MI001 standard and OIML R 49, where Q1 defines the minimum flow and Q4 defines the maximum flow. You can findmore informationoncatalog pages 3/126, 3/127 and 3/128 (for FM Fire Services). If you need more specific data, youcan go into our PIA Selector and use our sizing program online or download it. The link is below: https://pia-portal.automation.siemens.com/sie(cz1TSUQlM2FBTk9OJTNhRlRIVzlTN0FfUjNQXzAxJTNhYklmQm5ITlg4NkhSdDRkT3JYelhzTjdWU2Rqa2VwMkhoS2RGYkVBUS1BVFQ=)/z3_pia_portal/~flNUQVRFPTI3MjIuMDAyLjAxLjAxAA==?~okcode=EV_CAL Click on the Flow option and choose SITRANS FM. Best regards, Marco Antonio Camarena Amaro Product Manager, Siemens A/S Flow Instruments |
1/27/2015 2:17 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
|
Follow us on