7/16/2018 10:53 PM | |
Joined: 7/6/2018 Last visit: 5/26/2021 Posts: 5 Rating:
|
Hello, This is my first time posting to this forum, and I am new to PLCs and LOGO so apologize in advance for the lack of terminology. I am trying to measure the flowrate using a Flow Sensor from Omega, after trying to use both the High Frequency inputs and the analog inputs I was not able to pickup the signal. I called Omega and they said that the output voltage is too low to be picked up by the LOGO, so they are suggesting I get an amplifier to be able to see this signal. My question to this forum is, what is the minimum Voltage that the LOGO will pick up? They said that the peak voltage of the signal on the sensor is 30 mV. From my previous circuits experience I always though I could use pulse wave modulation to convert the analog signal into a pulse but I was not able to get the block to work. Thanks in advance for the help! |
7/17/2018 2:34 PM | |
Joined: 12/18/2014 Last visit: 6/27/2022 Posts: 27200 Rating:
|
Attached is an excerpt from the current manual. AttachmentLOGO! 8 manual 0BA8 2017_11 xxxx8-0BA0 pages 332-333.pdf (28 Downloads) |
Follow us on