4/24/2016 8:41 AM | |
Joined: 8/27/2006 Last visit: 4/23/2024 Posts: 719 Rating: (88) |
If it may help, I have attached the photo of the electronic card
AttachmentDesktop.zip (157 Downloads) |
The more you know, The more you know that you don't know |
|
4/24/2016 10:16 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello
You have not mentioned, what type of controller , you are using or plan to use. In my opinion, SIMOTION controllers like D425/D435 are best suited for such applications. Extensive libraries and Application examples are available for SIMOTION for Packaging machine applications. Here are some Links : SIMOTION Intelligent Infeed Packaging Machines SIMOTION Converting Library SIMOTION Utilities & Applications SIMOTION Rotary Knife Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to4 thankful Users |
4/24/2016 10:55 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
How the old system drives were controlled? Is this same machine mentioned in this post? From the application, it looks like both belts drive speeds are synchronised. |
4/24/2016 11:44 AM | |
Joined: 8/27/2006 Last visit: 4/23/2024 Posts: 719 Rating: (88) |
As I mentioned in my my post above, there was an electronic card in between the two which takes the reference from the main drive drive and do some "black box operations" and outputs this conditioned signal to the feeding belt drive. This is the same machine from the referenced post. The machine speed and the feeding belt speed are not speed synchronized only. It is more complicated than this. This is why I hoped anyone who did a similar application could help me. |
The more you know, The more you know that you don't know |
|
4/30/2016 2:54 PM |
|
Posts: 1529 Rating: (202) |
I must have missed that. He's got a 400 system? Damn, for the cost of an I/O card, he can get a D410. |
Follow us on